Making BIM even more efficient

Discover the data-light approach Grundfos uses to reduce system strain and improve workflows.

In this module, we’ll explore the data-light approach Grundfos uses to reduce the strain on systems while actively improving workflows. Let’s get started.

One of the major challenges of BIM is processing the significant amount of information that sits behind a project or data model. The more information that’s needed for a project, the greater the processing power systems need to navigate, amend, and manage it.

Often, BIM assets are constructed using the same 3D drawings created during product development and manufacturing. As a result, a lot of detail regarding the physical appearance of a product is automatically built into a BIM asset.

However, this information is not always relevant to all the stakeholders involved, such as engineers or contractors. It also makes the BIM significantly larger in data terms. Because of this, it can slow down the BIM project and reduce workflow efficiency for the end user. That’s why it’s essential for all elements in a project to be as data-light as possible.

To eliminate as much unnecessary detail as possible, Grundfos builds all BIM assets from scratch. Only the data that is absolutely necessary is included, reducing the computer processing required. It’s important to note that a more streamlined build does not mean an inferior BIM asset. Let’s take a closer look at how Grundfos builds BIM assets.

The Grundfos MAGNA assets feature exact geometry, the required piping and electrical connectors, and variant-specific mechanical, electrical and operational data. All Grundfos assets are also built to meet stakeholder demands. Let’s look at an example.

Specifying engineers have access to information on connection points, electrical loads, and head and flow. Energy consultants have access to operations parameters providing full fluid and energy simulation information, and service and maintenance engineers can retrieve necessary performance data.

Depending on each stakeholder’s needs and preferences, Grundfos BIM assets can be rendered in three different resolutions. All coarse, medium, and fine-rendered assets include full geometry and connection data while maintaining a data-light build for efficient, high-speed project workflow.

In BIM, building components are organised into reusable, parametric elements that can be customised and reused across projects. These elements are known as Revit families. At Grundfos, each Revit family comes as a type catalogue with all the standard product variants. This allows stakeholders to quickly switch between products when design conditions change.