Research And Insight

Constant curve

When there is a demand for constant flow and constant head, a speed-controlled pump can replace a throttle valve for adjusting the flow.

The speed can be adjusted between 25 % and 100 %.

This feature is especially beneficial in:

  • Heat surfaces
  • Cooling surfaces
  • Heating systems with 3-way valves
  • Air con. system with 3-way valves
  • Chiller pumps

The calculated control mode for constant curve is a feature of the Grundfos ALPHA range, MAGNA3 and TPE3 circulator pumps.

Related products

Find products from Grundfos related to this subject.

Related applications

Find applications from Grundfos related to this subject.