Research And Insight

Cooling jacket

A submersible pump cooling jacket enables a portion of the pumped liquid or an external liquid to be circulated around the motor stator housing. This absorbs excess heat by forced convection, ensuring efficient cooling of the pump.

Especially dry-installed pumps need special motor cooling. If needed, a submersible pump cooling jacket provides extra motor cooling if the pumped liquid is warm or if the pumps are required to pump continuously. The same applies if the liquid is pumped to below the level of the motor.

The cooling jacket can also be designed as an aluminium casing around the stator house. In this way the heat will be transferred to the pumped liquid via the aluminium casing.

Submersible pump cooling jackets for Grundfos dry-installed wastewater pumps for wastewater and groundwater applications.

Related products

Find products from Grundfos related to this subject.

Related applications

Find applications from Grundfos related to this subject.