Install & Operate
Ensure that your system functions at its best from day one. Find how-to guides, videos, FAQs and related services to help you with installation and operation of your Grundfos products.
The answers you need, when you need them
Access our self-service tools to search out a wide range of instant information on prices, availability, pump replacements and more.
Get help for your installing and operating needs
Look for how to guides here to find quick and easy guidance and support for all phases of your project. Discover a range of online engineering, installation and operation tools and up-to-date pump design information that can assist you in your work today, and help you work smarter over the long run.
Get answers to your questions about this situation
We have gathered frequently asked questions and their answers in one place. See the most frequently asked questions below or go to the Grundfos FAQ for a complete list of answers to your questions.
Can the pump be operated using a frequency converter?
Grundfos offers numerous speed-controlled pumps that are referred to as ‘E-pumps’ and which come equipped with Grundfos MGE motors with an integrated frequency converter. The manufacturing costs and material inputs are lower compared to pump solutions with external frequency converters. In addition, technical issues that may arise in connection with external frequency converters are avoided.
Finally, MGE motors have numerous additional features and advantages. In the event ...
Can the SP pumps also be operated in a horizontal position?
SP submersible pumps with a Grundfos or other submersible motor can be operated in any position from horizontal to vertical. The motor is arranged below the pump. A cooling jacket is generally required for these installation positions.
Do I have to follow the instructions for Grundfos pumps?
Yes, absolutely. The installation and operating instructions contain basic instructions which must be followed in connection with the installation, operation, and maintenance of the system. Hence, they must be read by the installer and the relevant personnel/owner prior to installation and commissioning. In addition, they must be available to personnel on site at all times.
Does the built-in excess temperature protection of the UPS pump need to be used?
If excess temperature protection is not properly connected or bridged, the pump may be permanently damaged. In addition, this will also void the pump's warranty.
Does the SQ/SQE have a soft start?
Yes, the pump has an integrated soft start feature in order to reduce start-up current, thus assuring even, continuous acceleration.
Does the SQ/SQE need to be manually reset after a certain number of automatic restart attempts?
In the event of a fault, the SQ will perform an unlimited number of restart attempts. As soon as the fault is no longer present, the pump will return to normal operation.
Become an expert in just a few clicks
Save time in your daily work by improving your skills, your know-how and your business with the online training platform ECADEMY.
Click on a course below to start your training now.
Grundfos Commissioning for me is top performance from day one
Grundfos specialists make sure that your system and pumps are fully compatible, that all pumps are installed and aligned correctly, and that the system is ready to go.
Related service offerings
Grundfos offers a variety of services all designed to give you peace of mind.
Prompt and reliable service wherever you are
With Grundfos service centres in more than 50 countries throughout the world, supplemented by more than 600 authorised Grundfos Service Partners, we’re never far away. If required, we ensure you get emergency access to service personnel as well.