FAQ
Question: How is the Capital investment compared to a conventional system with valves?
Answer:
Replacing valves with coil pumps and reducing primary pump size makes Grundfos Distributed Pumping cost the same or around 20% more than conventional systems.
Additional information:
Distributed pumping solutions replace larger centralised pumps and energy-consuming balancing and control valves with smaller intelligent pumps placed on each floor of the building. The result is substantial energy savings and a more comfortable indoor climate.