FAQ

Question: Which Pumps are used for Grundfos Distributed Pumping

Answer:

Grundfos Distributed Pumping is made possible with our connected pumps that gives optimal and intelligent distribution of chilled water to all terminal units.

Additional information:

Distributed Pumping solutions replace larger centralised pumps and energy-consuming balancing and control valves with smaller intelligent pumps placed on each floor of the building. The result is substantial energy savings and a more comfortable indoor climate.