Grundfos’ Engineering Expertise Revamps HVAC Systems in Dubai’s Iconic Skyscrapers

Case details

Topic: Commercial Air Conditioning
Location: Dubai, UAE

Grundfos supplied

  • LSV 200-150-305B, 37Kw + CUE
  • LSV 200-150-305B + CUE
  • Grundfos energy optimization solutions

Want to have PDF?

You can download the PDF or keep reading the case below.

The Situation

The HVAC system of two residential towers in Dubai faced persistent performance challenges due to a flawed initial design. The condenser pumps, positioned at a considerable distance from the cooling towers, were connected through a suction line with multiple bends, disrupting flow dynamics and resulting in severe cavitation.

This configuration led to excessive noise, vibrations, and frequent maintenance, undermining the system’s efficiency. Compounding the issue, the pumps were oversized and operating far from their Best Efficiency Point (BEP), leading to increased energy consumption, reduced reliability, and a heightened risk of chiller overflow, prompting the need for a smarter, more efficient solution.

By redesigning the suction side piping layout and optimizing the system hydraulics, we were able to eliminate cavitation, cut energy use, and significantly improve overall reliability. It's a clear example of how smart engineering can solve complex challenges and deliver lasting efficiency.
Velon Saldanha, Aftermarket Sales Engineer

The Solution

Following a comprehensive Pump Audit, Grundfos engineers gained in-depth insight into the system’s limitations and proposed a complete redesign and right-sizing of the condenser pumping system. A key corrective step was repositioning the pumps closer to the cooling towers, improving overall system hydraulics and resolving the persistent suction-side cavitation issues.

Grundfos selected new pumps tailored to the revised layout and actual performance needs of the condenser circuit. To enhance flexibility and control, external Variable Speed Drives (VSDs) were integrated, allowing the system to adapt to fluctuating load conditions. By addressing low Net Positive Suction Head (NPSH) and optimizing the pipework, the new design enabled the use of smaller, more efficient pumps, reducing motor size from 55 kW to 37 kW. This resulted in notable energy savings and a substantial reduction in operational costs, while improving overall system stability and reliability.

The Outcome

With accurately resized condenser pumps tailored to the installation’s true flow and head demands, the system saw a substantial drop in energy consumption and a dramatic reduction in the risk of chiller overflow. Grundfos’ complete redesign of the condenser circuit, including the strategic repositioning of pumps, successfully eliminated the low NPSH conditions that had been causing persistent cavitation.

The result was a smoother, more stable operation with significantly improved system efficiency, lower maintenance requirements, and reduced operational costs—delivering long-term value and reliability for the residential towers.

Up to 632,034 kWh

Annual energy savings

95,7 tonnes

Annual CO₂ reduction

278,095 AED

Annual cost savings

Overview of products featured in this case study

Learn which products were used and how they contributed to the case results.

 

Discover related applications

Learn more about the applications which are mentioned in this case story.