In the Middle East, where ambient temperatures routinely exceed 45°C and urban development is accelerating at an unprecedented pace, thermal management has emerged as a critical pillar of sustainable infrastructure. From dense metropolitan centers to visionary smart cities, the region is increasingly turning to district cooling as the preferred solution for large-scale climate control—one that balances energy efficiency with environmental responsibility.

Driving this transformation is Grundfos, a global leader in advanced pump technology and water solutions. With a legacy of engineering excellence and a deep commitment to sustainability, Grundfos is not merely supporting the region’s growth, it is enabling it. By delivering intelligent, high-performance pumping systems, the company is helping cities stay cool while laying the foundation for a more resilient and energy-conscious future.

District cooling: The engine for sustainable urbanism

District cooling systems operate by distributing chilled water from a centralized plant to multiple buildings via a network of pre-insulated underground pipelines. This centralized model replaces conventional HVAC systems, offering superior energy efficiency, reduced operational complexity, and optimized load distribution. In climates like the Middle East, where cooling demand can represent up to 70 percent of peak electricity consumption, district cooling can reduce energy usage by 50 when integrated with thermal storage technologies. 

Beyond technical performance, district cooling also enhances urban design by reducing noise, freeing up rooftop space, and enabling greener, more open environments. It is both a mechanical solution and a strategic enabler of sustainable urbanism.

Grundfos: Delivering engineering excellence

Across the Middle East, Grundfos has become a trusted partner in building the infrastructure that powers district cooling. The company delivers digitally intelligent, space-optimized, and energy-efficient pumping systems that align seamlessly with the region’s sustainability goals.

When a district cooling plant in Dubai faced tight timelines, limited power, and space restrictions, Grundfos delivered a bespoke solution built for performance and sustainability. Equipped with high-efficiency axially split case, double suction-double volute pumps LS and LSV pumps and IE4 motors, the system achieved up to 87.5% efficiency—reducing both energy consumption and capital costs. Enhanced with Belzona coatings and supported by Grundfos’s collaborative project management, the plant became a benchmark in sustainable cooling, aligning with Dubai’s Clean Energy Strategy 2050, which targets 75% clean energy by mid-century.

This standout project exemplifies Grundfos’s end-to-end support model, where the company collaborates closely with clients, consultants, and contractors from design to handover. The result: a district cooling plant that not only meets sustainability benchmarks but also sets new standards in operational excellence.

Futuristic architecture meets smart cooling

The Middle East’s architectural evolution demands mechanical systems that match the region’s ambition for innovation, sustainability, and intelligent design. As buildings become more complex and digitally integrated, cooling infrastructure must evolve in parallel delivering not only thermal comfort but also operational efficiency and spatial adaptability. Grundfos addresses these challenges with engineered pumping solutions that integrate seamlessly into high-performance environments. 

Designed with compact geometries, these systems minimize mechanical room footprints and maximize usable space within dense urban developments. Embedded digital monitoring capabilities enable predictive maintenance and real-time performance optimization, ensuring continuous reliability and reduced lifecycle costs. Furthermore, the modular architecture of Grundfos’s systems allows for scalable deployment, accommodating phased construction and future urban expansion.

In Saudi Arabia, Grundfos is actively contributing to the Kingdom’s Vision 2030 by deploying energy-efficient, digitally enabled pumping solutions across next-generation commercial developments. These systems are engineered to support smart building ecosystems, interfacing with advanced building management platforms to deliver granular control over energy consumption and system diagnostics. By aligning with national sustainability goals and digital transformation strategies, Grundfos reinforces its role as a strategic partner in shaping the infrastructure of tomorrow.

Grundfos is redefining how the Middle East stays cool; powering smarter, more sustainable cities with intelligent pumping systems that form the backbone of modern urban life.
Gaurav Kapoor, Regional Key Account Manager District Energy, Grundfos Commercial Building Services - IMEA

Sustainability at scale

The commitment to sustainability extends beyond energy efficiency. By centralizing chilled water production and distribution, Grundfos-powered district cooling systems significantly reduce the carbon intensity of urban infrastructure. Industry estimates suggest that district cooling can lower electricity consumption for cooling by up to 50 percent. Grundfos’s high-performance pump technologies are engineered for maximum hydraulic efficiency and minimal environmental impact, supporting national frameworks such as the UAE Water Security Strategy 2036 and Saudi Vision 2030. In addition, the company contributes to regional water resilience through its participation in the Water Resilience Coalition, advocating for responsible water management in some of the world’s most water-stressed regions. 

Grundfos’s leadership is not confined to engineering, it extends into policy advocacy and stakeholder collaboration. Through platforms like WETEX, DC Dialogue the company facilitates dialogue among government leaders, industry experts, and innovators to promote sustainable water and energy practices. These engagements have led to policy recommendations for district cooling integration in urban master plans and the development of digital infrastructure pilots featuring AI-driven fault detection and energy optimization. This collaborative approach underscores Grundfos’s belief that sustainability must be built collectively, with all stakeholders contributing to the cities of tomorrow.

The road ahead: Cooling the future 

Looking ahead, the role of district cooling in the Middle East is set to expand dramatically. By 2030, it is projected to meet 30 percent of the Gulf Cooperation Council’s cooling demand, potentially offsetting 200,000 barrels of oil equivalent per day and eliminating the need for 20 gigawatts of new power generation capacity. 

With over 75 years of engineering expertise, a portfolio of intelligent, energy-optimized solutions, and a proven track record in large-scale deployments, Grundfos is positioned to lead this transition. As urban landscapes continue to evolve, Grundfos remains at the forefront—engineering the thermal backbone of sustainable cities and cooling the future, one drop at a time. 

Meet our expert:

Gaurav Kapoor:
Regional Key Account Manager
District Energy, Grundfos Commercial Building Services - IMEA

Gaurav Kapoor is Regional Key Account Manager – IMEA for District Energy, with over 15 years of experience in the pumping industry. Gaurav specializes in optimizing water and HVAC systems, applying strong technical expertise to complex challenges, specifically on large district and campus cooling projects. He is focused on advancing sustainable and energy-efficient pumping solutions.

This article was published in Construction Week Middle East in 2025. To view it on the Construction Week website please click.