FAQ

Question: When does the MQ switch off?

Answer:

The flow switch only causes the MQ to switch off automatically during normal operation if the flow rate drops below 0.07 m³/h. If the flow rate drops below the required level, the pump switches off after 12-15 seconds. It is also possible to switch the pump off manually using the ON/OFF switch.

The MQ also switches off after an overtemperature alarm or dry running alarm triggers.

Additional information:

Enhance your knowledge

Find out how to get reduced energy consumption, increased comfort and unsurpassed operational reliability for your application. Read our customers' stories about how they benefit from the Grundfos approach to intelligence, water and energy, or search Grundfos research & insights for more learning materials, articles, white papers, videos and much more that benefit your solution.