Case details

Topic: Commercial Air Conditioning
Location: UAE

Grundfos supplied

  • End suction, back pull-out, NB pumps
  • HVAC Control MPC panel
  • Energy optimization solutions

Want to have PDF?

You can download the PDF or keep reading the case below.

The Situation

3 premier educational institutions in UAE were facing persistent challenges with their primary and secondary chilled water systems. The existing pump setup, especially on the secondary side, was found to be oversized and prone to cavitation issues, resulting in unstable operations and energy inefficiencies.

During an initial assessment, the Grundfos team discovered that the pumps were operating significantly outside their optimal performance curve and far from the Best Efficiency Point (BEP). These findings raised concerns about long-term reliability, excessive energy consumption, and potential damage to system components.

To resolve these challenges,, Grundfos conducted a comprehensive Energy Audit to quantify the energy-saving potential and propose tailored improvements aimed at restoring system balance, efficiency, and performance reliability across all three school facilities.

Our customized HVAC solutions enabled pump downsizing and showcased our energy optimization expertise, delivering significant energy and cost savings.
Velon Saldanha, Aftermarket Sales Engineer

The Solution

To address the inefficiencies and restore optimal system performance, Grundfos designed a customized pumping solution tailored to the actual cooling requirements of the schools. The primary objective was to deliver measurable energy savings while significantly lowering operational costs.

A key aspect of the solution involved resizing the pumps to precisely match the flow and pressure demands of the installation, thereby eliminating the inefficiencies associated with oversized units. To further enhance system responsiveness and efficiency, frequency drives provided by the project’s ESCO partner were integrated with a Grundfos CU352 controller. This intelligent control system enabled real-time performance modulation, allowing the pumps to dynamically adjust to cooling demand fluctuations thus ensuring stable, energy-efficient operation at all times.

The Outcome

The replacement of outdated pumps with right-sized Grundfos solutions significantly improved the HVAC system’s performance, resulting in a substantial reduction in energy consumption and lower electricity costs. By eliminating cavitation and ensuring smoother, more stable operations, the solution also reduced maintenance expenses and improved the overall reliability of daily system performance.

Executed under an ESCO performance contract, the project required no upfront capital investment from the customer. All upgrade costs—including maintenance and spare parts—are fully covered by the energy savings achieved, making this a cost-effective, risk-free solution for the institutions.

Up to 630,457 kWh

Annual energy savings

315,2 tonnes

Annual CO₂ reductions

277,401 AED

Annual cost savings

Overview of products featured in this case study

Learn which products were used and how they contributed to the case results.

 

Discover related applications

Learn more about the applications which are mentioned in this case story.