Research And Insight

Pressure holding pumps

Pressure holding is a system for maintaining a constant static pressure is used in heating and cooling systems to order to ensure uninterrupted operation. This can be achieved in more ways than one.

In smaller boiler-supplied heating systems, constant static pressure can be achieved with an open expansion vessel. This vessel is placed at the highest point in the system. A static pressure corresponding to the physical height is thus created.

In smaller closed systems, constant static pressure can be achieved with a pre-pressurised expansion vessel. Using a pre-pressurised expansion vessel in larger systems would be inconvenient due to large size necessary.

Therefore, pressure holding systems are used in larger systems. These can contain a pressure expansion vessel, with an attached compressor or a pressure holding pump. The compressor or pump automatically ensures that the correct static pressure is maintained in the system by regulating vessel pressure.

A pump-based pressure holding system is comprised of one or more pumps connected in series. The pumps can be fitted with a speed regulator, e.g. frequency converter, to maintain correct pressure within the system. In this case a pressure expansion tank is not necessary because the pumps themselves are able to regulate the pressure. 

Pressure holding systems using speed-regulated pumps are superior to systems that employ expansion vessels. In the latter case, a constant-speed pump that maintains a constant flow can give rise to pressure surges when the pump starts and stops. Furthermore, a pressure holding system requires less physical space since there is no expansion vessel.

A pressure expansion tank combined with a pressure holding pump can be used to remove air from process water. A small volume of water is filled into the container, which is not pressurised. When the pressure falls to atmospheric pressure, most of the air is released. A similar volume of water is pumped back into the system by a pressure holding pump to maintain the desired pressure in the system.

The Grundfos circulator pump range, with or without variable speed control, are ideal as pressure holding pumps.

Related products

Find products from Grundfos related to this subject.

Related applications

Find applications from Grundfos related to this subject.