FAQ

Question: Who can commission a Grundfos Distributed Pumping solution?

Answer:

Our highly trained Grundfos Service and Solutions Engineers will do the commissioning of the distributed pumping solution, which includes: 

  • A pre-commission visit, ensuring the installation of the pumps are in order.
  • Initial configuration of the pumps according to the specifications in the design.
  • Solution commissioning, ensuring the whole system is operating as per designed.

Additional information:

Distributed pumping solutions replace larger centralised pumps and energy-consuming balancing and control valves with smaller intelligent pumps placed on each floor of the building. The result is substantial energy savings and a more comfortable indoor climate.