Grundfos Water Treatment Europe (former EUROWATER) has designed and manufactured the water treatment solution for the world's first commercial plant that increases biogas production through electrolysis and biological methanisation.
Key topics:
- Innovative, containerised water treatment solution
- Energy and resource efficiency
- Environmental impact
The energy and fibre network group Andel and the global biogas producer Nature Energy are behind the Power-to-gas plant in Glansager on Als in Denmark.
Here, excess electricity from wind turbines is utilised to increase biogas production while reducing CO2 emissions. This is achieved by converting CO2 into biogas through the addition of hydrogen. Hydrogen production is based on alkaline electrolysis (AWE) using ultrapure water as feedstock.
The water treatment consists of softening followed by membrane filtration and membrane degassing. The solution also includes a pumping station and CIP unit.
Treatment steps in the solution
The 3 x 3 MW alkaline electrolyser relies on a stable supply of 1,600 litres of ultrapure water per hour with a conductivity below 5 μS/cm.
The raw water is city water that has already undergone aeration and sand filtration. To achieve the desired water quality it undergoes additional purification to eliminate metal ions, organic substances and CO2. The water treatment therefore consists of the following treatment steps:
- Softening as a pre-treatment for the reverse osmosis system to avoid fouling and limescale deposits in the membranes.
- Membrane filtration with a double-pass reverse osmosis system, where ions and organic substances are removed from the water, resulting in demineralised water. This system incorporates Grundfos energy-optimised e-pump, which significantly reduces energy consumption compared to traditional pumps.
- Membrane degassing ensures efficient CO2 removal as the reverse osmosis system does not remove dissolved gases.
The solution consists entirely of standard Grunfos Water Treatment Europe's units that are commonly used in power plants. The quality of boiler water in power plants closely aligns with the water quality specifications needed for electrolysers.
The water treatment solution is installed in a 20' container. The solution comes with all internal piping and wiring, pre-assembled at the factory.
Mobile solution
The water treatment is installed in a 20' container as an alternative to constructing a dedicated building for the solution. A containerized solution provides a flexible and mobile solution where fixed maintenance costs can be minimised.
The solution is assembled, factory-tested and delivered with all internal piping and electrical connections. This significantly reduces installation time as the solution is ready to use upon delivery.
Facts
Related case stories
Read related stories from customers who have also benefited from a Grundfos solution.
No hydrogen without water
The transition to green energy is not just about production; storage and distribution are equally important. ‘Green hydrogen’ production meets this challenge. And water plays a crucial role in this process.
Hydrogen production involves moving and treating large amounts of water to meet requirement for makeup water, refinement loops, ultra-pure water treatment or cooling process applications. Our water technology expertise helps you move and treat water in the right way: reliably, sustainably and cost-efficiently.