FAQ

Question: How much hydrogen can I produce from my water?

Answer:

Water contains two atoms of hydrogen and one oxygen atom. Because oxygen is 16 times heavier than hydrogen, it takes up most of the mass in a water molecule. 89% of the mass is oxygen and 11% is hydrogen. This means that to produce 1 kg of hydrogen, 9 kg of water are required. In reality, 10-13 kg of water are required due to losses and inefficiencies.

Additional information:

Learn about efficient water treatment to enhance electrolyser systems

Whether you're looking for an in-depth exploration of refinement loops and seawater usage in hydrogen production, or just a brief overview of the importance of water treatment, our whitepapers have you covered. Dive into our comprehensive resources to uncover the benefits of proper water treatment in the hydrogen production process.