Odense University Hospital (OUH) has reduced its annual water consumption by 10,000 m³ through a centrally located water treatment plant that has been optimised for water, salt, and energy consumption.
Topic: Water and energy savings
Location: Odense, Denmark
Industry: Hospitals, healthcare
Technical data:
- Flow: 50 m³/h softened water
- Flow: 3 x 7 m³/h demineralised water
The situation
Thousands of patients are treated at Odense University Hospital (OUH) in Denmark every day. It is OUH's ambition to ensure that every patient receives expert treatment and that they feel well looked after in terms of nursing and care. To meet this ambition, access to water of the right quality and in the right place is an important factor.
When OUH decided to install a new water treatment plant, the hospital wanted a robust solution focusing on operational safety and economy. To meet these requirements, Grundfos needed to utilise new and energy-efficient technologies to minimise water and energy consumption.
The solution
Water and salt-saving softening plant
OUH chose a softening plant of the type STFA comprising two tanks with ion exchange media. The softening plant has a total treatment capacity of 50 m³/h and is designed with a distributor section ensuring a uniform and even flow, thereby fully utilising using the full capacity of the media filter.
The regeneration of the softening plant represents a large part of the total operating costs. Various special features can help to minimise both the consumption of water as well as the salt for regeneration:
- Monitoring of the regeneration water quality
- Reuse of regeneration water from the various regeneration phases to the greatest possible extent
- Plant designed to use exactly the amount of salt needed regardless of ambient temperature
Part of the softened water is used as process water in the washing machines, dishwashers and bedpan washers. The remaining volume is processed in three RO systems.
Water and energy saving reverse osmosis system
OUH chose three RO systems of the type RO-PLUS, which is characterised by offering a high recovery rate of up to 90 %. In comparison, most other types of RO systems have a recovery of about 75 %.
RO-PLUS is designed for higher recovery without compromising on water quality or reliability of operation. In theory, this might sound simple to achieve, but in practice it can be problematic if you do not have the right experience and know-how. Each RO system is designed for a performance of 7 m³/h.
The high recovery not only results in significant savings of water consumption, but also of energy consumption. Energy consumption per m³ is reduced by utilising a larger quantity of the inlet water.
The demineralised water is used for steam boilers, autoclaves and in the laboratories.
The outcome
At OUH, there are large fluctuations in water consumption during the day. To obtain an optimum production flow, the treated water is stored in a buffer tank. This reduces both electricity, water and salt consumption significantly.
To avoid bacteriological contamination, the water from the buffer tank is continuously recycled through a UV system and a reverse osmosis system. UV light disinfection effectively eliminates all microbiological growth in the water by destroying the microorganisms' DNA, i.e. bacteria, viruses, algae, and fungi. The RO membranes remove all organic matter and thus also act as a hygiene barrier.
Compared with the old water treatment plant, the new water treatment plant at OUH achieved such large operating savings that the payback period was approximately one year.
Process chart illustrating the principle of water treatment at OUH and hospitals in general
Grundfos supplied:
- Softening unit type STFA 30 duplex
- Testomat online hardness measuring
- Equipment for reuse of backwash water
- 3 x reverse osmosis units with high water-recovery technology type RO-PLUS
- Single-pass reverse osmosis unit type B1-1
- UV-disinfection unit
How can we help you?
Whether you’re looking to buy a product or simply seeking advice from a Grundfos expert, we are more than happy to help you get the most out of your water treatment solution! Feel free to get in touch if you need support.