Ending the wait: How saving hot water can power households, the economy, and the environment

The problem: Wasting water while waiting

Every day, millions of Americans wait between 30 seconds to 2 minutes and even longer for hot water to reach their faucets or showers. During that time, clean, potable water goes straight down the drain. For the average home, this adds up to 3,650 to 13,505 gallons of water wasted per year – just waiting for hot water.

Download the full infographic

Get the full overview by downloading our interactive infographic.

When scaled across the U.S., this translates to a staggering 430 billion to 1.59 trillion gallons of water wasted annually, even when accounting for the 10% of homes that already have instant hot water systems.

To put these staggering numbers into context, an Olympic-sized swimming pool contains an estimated 660,000 gallons of water, meaning that somewhere between 0.65 million and 2.4 million Olympic-sized swimming pools go down the drain every year, simply waiting for hot water.

The opportunity: Saving households water and money

By eliminating the wait for hot water, American households could dramatically reduce their water waste and lower their utility bills. Based on average national water rates (~$0.004/gallon), households could save between $15 and $54 per year. Nationwide, the total economic savings on water bills would be between $1.72 billion and $6.37 billion annually.

This isn’t just a theoretical estimate. In December 2024, I installed a Grundfos ALPHA COMFORT SYSTEM, significantly reducing the time it takes for hot water to reach faucets and showers. In just the first two full months, I saved 1,223 gallons of water compared to the same period last year – translating to a $5.08 reduction on my water bill. Projected across the whole year, that’s approximately 7,338 gallons of water saved and $30.48 off my water bill over 6 billing cycles.

That places me comfortably in the middle of the estimated range for potential household water savings (3,650 to 13,505 gallons annually), providing a clear and relatable example of how real-life usage lines up with the broader national data. It’s a simple yet powerful reminder that individual households can make a measurable impact with accessible technology.

Full disclosure: I work for Grundfos. That said, I’ve seen countless examples of water and monetary savings like this – across different homes, geographies, and customer types – over many years. These outcomes are real, repeatable, and impactful. The combination of small savings in the household can become a powerful force for change on a national scale.

And while hot water recirculation may be the unsung hero of household water efficiency, it’s important to recognize its evolution. In the past, these systems focused mainly on saving water but often came with a significant trade-off: energy inefficiency. In many cases, older models would run continuously, consuming unnecessary electricity and forcing water heaters to work harder – sometimes increasing energy use by up to 50%. Thankfully, those days are behind us. Today’s smart recirculation systems use ECM (electronically commutated motor) technology, intelligent sensors, and programmable timers to deliver hot water efficiently while minimizing energy use. In short, we no longer have to choose between saving water and saving energy – we can do both and do it smarter. And hot water recirculation isn’t the only solution.

There are other simple, proven ways for households to conserve water without sacrificing comfort or convenience. Low-flow fixtures like aerated faucets and high-efficiency showerheads reduce usage without compromising performance. Smart irrigation controllers adjust watering based on weather and soil conditions. And fixing common household leaks – often silent and unnoticed –  can prevent thousands of gallons of wasted water each year.

In addition to water bill savings, households can expect to save on sewer/waste water charges. Most municipal sewer bills are based on water consumption, meaning that any reduction in water use translates directly into reduced sewer fees. At an average sewer rate of approximately $6.50 per 1,000 gallons, households could save an additional $24 to $88 per year. Nationally, this equates to between $2.8 billion and $10.3 billion in sewer bill savings annually.

Total combined utility savings: $4.5 billion to $16.7 billion per year!

These figures demonstrate the full economic impact of ending the wait for hot water. The savings go directly into homeowners’ pockets, strengthening household finances while supporting national water and energy conservation goals.

A bigger impact than you think

Eliminating the wait for hot water does more than save time, water, and money. It reduces hidden energy demand and emissions at a national scale. Every gallon of clean water delivered to a home takes energy to produce, especially when sourced from groundwater or surface water systems. When we waste hot water, we’re not just wasting a resource – we’re throwing away the electricity used to create it.

In fact, the electricity used to produce the water we waste while waiting for it to warm up ranges between approximately 745.6 million and 2.76 billion kilowatt-hours each year. That’s enough energy to power between 70,000 and 260,000 U.S. homes annually.

This is not just about personal savings – it’s about reallocating meaningful national energy capacity toward more productive use. Reducing this demand could ease pressure on aging grid infrastructure, cut utility costs, and accelerate progress toward decarbonization.

The bigger picture: Fueling economic growth and sustainability

Reallocating 430 billion to 1.59 trillion gallons of water from waste to productive use opens doors far beyond the household. This is not about needing new water sources – it’s about making better use of what we already have. By stopping the waste of hot water in homes, we unlock a transformative opportunity to reallocate clean, potable water toward vital sectors of the economy that are already thirsty for growth.

Agriculture, which consumes nearly 80% of freshwater in many states, could benefit immensely. Even a fraction of the saved water could irrigate millions of additional acres, increasing crop yields, stabilizing food prices, and making American farms more resilient to drought. Industry –  particularly sectors like semiconductors and manufacturing – could expand without hitting water supply ceilings.

For example, semiconductor plants require billions of gallons of ultra-pure water each year, and data centers rely on millions of gallons daily for cooling. This reallocation could power hundreds of new facilities without straining local supplies.

New technologies such as vertical farming, clean hydrogen production, and biomanufacturing are also water-intensive. With the right allocation, we can future-proof the economy, fuel innovation, and attract investment in next-generation industries that define the digital and low-carbon era.

Most importantly, this isn’t a hypothetical scenario. The water already exists – it’s simply misallocated through inefficient hot water systems. By adopting smarter technologies like recirculation pumps, better insulation, and more efficient water heaters, we can redirect this water where it’s needed most.

It’s a strategic, no-regrets investment in America’s future – where household comfort translates into national competitiveness.

A win-win solution for America

The case is clear: solving the everyday inconvenience of waiting for hot water can translate into nationwide benefits. Homeowners save money. Communities preserve a vital resource. Industries grow stronger. And the country gains resilience and an economic edge. It’s a rare opportunity where comfort, conservation, and competitiveness go hand-in-hand.

Final thoughts: A no-brainer for America

At the end of the day, this is a no-brainer. Saving water is a win-win for everyone involved. It benefits homeowners by lowering their utility bills and improving comfort. It helps communities conserve a precious natural resource. And more importantly, it creates the foundation for strong, sustained economic growth.

Water is not just an environmental issue – it’s an economic engine. The ability to redirect wasted water into agriculture, high-tech industry, manufacturing, and innovation allows us to unlock new jobs, secure supply chains, and power the industries that will define America’s future. This isn’t just about conservation – it’s about economic expansion, global competitiveness, and national resilience.

We don’t need to invent anything new. We already have the tools and technology to make this shift today. What’s needed now is the awareness, the will, and the leadership to act. Let’s seize this opportunity, and ensure that every gallon of water serves a purpose – from the faucet to the factory.

Let’s not waste another drop of potential.

Related products

Find products from Grundfos related to this subject.

Related applications

Find applications from Grundfos related to this subject.

Other related articles and insights

Find related articles with research and insights from Grundfos.