Grundfos Delivers Flexible Treatment and Proven Reliability at the Little Falls Wastewater Treatment Plant.

Introduction

Five years after commissioning its new Tri-Oval Oxidation Ditch System, the Little Falls, MN Wastewater Treatment Plant is delivering reliable treatment, strong phosphorus performance and operational flexibility. The plant consistently operates well below its treatment limits, most notably its 12-month rolling Total P (phosphorus) discharge limit as defined by the EPA, providing operators with confidence in the system’s ability to meet regulatory requirements. For the plant’s operators and wastewater supervisor, that performance is a source of pride. The system provides the reliability and control they need to confidently treat wastewater before it is discharged to the Mississippi River, helping protect an important regional waterway. Flexible aeration and minimal maintenance have also made the system straightforward to operate and maintain.

The mixing looked amazing. We knew strong mixing would be a requirement for the new treatment system if we wanted to maintain the same footprint.
Matt Streit, Wastewater Superintendent for Little Falls

The Grundfos Tri-Oval Oxidation Ditch System (above) features two treatment trains designed to deliver reliable biological treatment, strong mixing and operational flexibility within the plant’s existing footprint.

The System Upgrade

The Little Falls Wastewater Treatment Plant serves the city’s residents, businesses and local industries, including food and beverage and pet food manufacturers. The plant treats approximately 1.0 MGD of wastewater under typical conditions and has a maximum flow capacity of 2.6 MGD. Before its 2021 upgrade, the facility relied on a high-rate trickling filter and aeration basin with coarse-bubble diffused air. As the equipment and treatment process aged, the city needed to modernize the facility while also preparing to meet a new phosphorus requirement of 2,652 kg/year on a 12-month rolling average.

The city wanted a treatment system that could work within the existing site footprint while providing effective mixing in deep basins and greater operational flexibility. Reducing energy consumption during periods of lower demand was also important, as was the ability to adjust aeration in the future if additional nitrogen treatment requirements were introduced. 

Working with SEH engineering, the city evaluated several treatment approaches, including carousel and diffused-air technologies. The project team visited the local Grundfos facility in Chaska, MN as well as an operating Tri-Oval Oxidation ditch in close by Renville, MN to see the technology in operation. The team was particularly impressed by the mixing that the Triton aerators provided. “The mixing looked amazing.”, recalled Matt Streit, Wastewater Superintendent for Little Falls. “We knew strong mixing would be a requirement for the new treatment system if we wanted to maintain the same footprint.” The combination of strong mixing, operational flexibility and ease of equipment access ultimately made the Grundfos Tri-Oval system the preferred solution for the plant.

The Solution

Performance Against Permit

SEH Engineering & the City of Little Falls ultimately chose Grundfos’s Tri-Oval Oxidation System to meet the needs of| their new system requirements. Grundfos provided a two-train Tri-Oval Oxidation Ditch System, with each train equipped with two 60 HP Aire-O2 Triton Process Aerator/Mixers, Universal Bridge Mounts, a dissolved oxygen (DO) probe and Primex control panels. The Triton aerators provide both aeration and mixing from a single unit, allowing operators to manage the biological process based on actual treatment requirements. The plant operates at approximately a 2 mg/L DO setpoint, while variable-speed operation allows operators to reduce aeration during periods of lower oxygen demand, reducing energy consumption. The system also provides on/off aeration capability, giving operators additional flexibility as treatment requirements change. This could become particularly valuable if the plant faces future nitrogen treatment requirements that require more precise control of aerobic and anoxic conditions.

Results

Five years into operation, the Tri-Oval system has provided Little Falls with the treatment performance and operational flexibility the city was seeking. The plant consistently operates well below its regulatory limits, namely, Total P discharge limit of 2,652 kg/yr (12 mo. rolling average) as defined by the EPA, providing a significant margin of compliance and confidence in the treatment process.

For the operators, that reliability matters every day. The plant team takes pride in knowing the system is performing as intended and that the wastewater leaving the facility is receiving the treatment necessary to help protect the Mississippi River. Operators routinely monitor BOD, TSS, phosphorus, pH, dissolved oxygen and nitrogen, providing visibility into overall treatment performance and allowing the process to be adjusted as conditions change.

Mixing

The Triton aerators have demonstrated strong mixing performance in the plant’s 23-foot-deep oxidation ditches. Operators have verified that the basins remain completely mixed to the bottom, helping maintain consistent biological treatment throughout the process.

Operational Flexibility

Variable-speed aeration gives operators the ability to match aeration energy use to actual process demand. During periods of lower demand, aeration can be reduced, helping limit unnecessary energy consumption. The ability to turn aeration on or off also provides flexibility for future process changes and potential nitrogen treatment requirements.

Maintenance

When asked how the maintenance of the Tri-Oval System has gone over the last 5 years, Matt Streit (Wastewater Superintendent) responded “We haven’t had to do anything to them.” Intimate access to the aerators via Grundfos’s patented Universal Bridge Mounts have simplified operation and maintenance by allowing the aerators to be raised for inspection and service using the winch track system. Routine maintenance consists greasing the mixer motor and universal joint, and not much else. The plant has not needed to replace the aerator bearings, further demonstrating the system’s reliability in operation.

The facility has two oxidation ditches (above) , but operates only one at a time, allowing the second ditch (right) to remain offline as a backup or for maintenance.

Grundfos Delivered

Tri-Oval Oxidation Ditch System – Two treatment trains designed to provide reliable biological treatment, strong mixing and operational flexibility within the plant’s existing footprint.

Aire-O2 Triton® Process Aerator/Mixers – Four 60 HP surfacemounted aerator/mixers, with two units per train, providing both aeration and complete mixing in the 23-foot-deep oxidation ditches.

Universal Bridge Mounts – Patented mounting systems that provide convenient access to the Triton aerators for inspection and maintenance.

Dissolved Oxygen Probes and Primex Control Panels – Process monitoring and controls that enable variable-speed and on/ off aeration to match treatment requirements and improve operational flexibility.

Summary

Five years after commissioning, the Tri-Oval Oxidation Ditch System has become a dependable part of Little Falls’ wastewater treatment operation. With strong treatment performance, complete mixing, flexible aeration and minimal maintenance, the system gives operators confidence in the treatment process and pride in the role they play in protecting the Mississippi River.