Case

APC No moving parts, No problem

Customer statement from Kevin Lemke, Staff Product Manager - InRow Cooling, APC by Schneider Electric :

The Situation

“APC by Schneider Electric is a leading provider of precision cooling solutions for IT environments. The cooling solutions we provide are integrated with active response controls that monitor and react to changes in the IT environment.

As a part of the control system, we monitor several sensors and adjust the cooling units performance to ensure stable inlet temperatures to the IT equipment. A performance point that we relay to the end user is the actual cooling capacity of the unit. This provides visibility to the amount of cooling that is being provided by individual units or groups. IT managers can use this data for planning the deployment of server assets based on available capacity locations.”

 

The Grundfos Solution

“One way that we are able to capture the data required is by equipping each InRow® cooling unit with a Grundfos flowmeter. This allows us the ability to read the flow rate of fluid travelling through the unit and combine that with the entering and leaving water temperature data to calculate the current cooling
capacity of the unit or group of units.”

 

The Outcome

“The Grundfos flow meter’s lack of moving parts provide us with a reliable flow sensing solution to enable our controls to provide a predictable solution for an unpredictable environment.”

Other related cases

Read related stories from customers who have also benefited from a Grundfos solution.