With an estimated payback period of just over two years and a 90 % reduction in operating costs, MEC did not hesitate long before pressing the button to order a new water treatment plant from Grundfos.

Introduction

MEC is situated just outside Holstebro in Denmark. MEC is a combined waste and biomass-fired heating and power plant, which supplies district heating and electricity to households in two Danish municipalities. Since the commissioning in 1993, a water treatment plant consisting of a reverse osmosis system with subsequent service-regenerated mixed bed plant has produced deionate for the power plant's high-pressure boiler. The boiler produces steam for the plant's steam turbine.

Unfortunately, the water treatment plant had very high operating costs during its useful life, so when engineer Jørgen Pors-Nielsen in 2018 became operations manager for turbine operation and water treatment, it was decided to take care of this.

Nourished with Grundfos water

Jørgen Pors-Nielsen, the 32-year-old operations manager, almost grew up with a pipe wrench in his hand. As a child, he lived in a disused school with its own water supply – nothing less than a NSB sand filter from Grundfos, which he and his father serviced.

Operations Manager at MEC, Jørgen Pors-Nielsen.

Here he also built a small mobile forge from an old Nilfisk vacuum cleaner with a playing card as a regulator (to replace the prototype with double bellows), where he forged small knives, arrowheads, and nails. It was obviously a completely natural thing for Jørgen to train as a locksmith and then an engineer.

After graduating, he worked for a period for DONG (now known as Ørsted Energy), but after a few years was hired as operations manager at MEC. He even sits on the board of the district heating plant that supplies his own home.

New plant with RO and EDI

When Jørgen had agreed with the management on the improvement of the water treatment situation, he inquired within his network. Here he was advised to contact Grundfos; a name that for Jørgen evoked positive memories from his childhood home. After a good conversation at the Ajour trade fair 2019, the dialogue started on a solution proposal: A double-pass reverse osmosis system (DPRO) with subsequent EDI system, an electrically regenerated mixed bed plant used for total demineralisation of water.

The upgrade from single-pass to a double-pass system provides a much better operation of the EDI system resulting in significantly longer operating time between regenerations for the subsequent mixed bed plant.

The actual dimensioning and design of the plant was carried out in close cooperation between MEC and Grundfos. In addition to the technological solution, there were practical things to consider. The location of the plant should match existing foundations and connections. The plant was required to communicate with the existing control. Thanks to 85 years of experience and some of the most skilled employees in the industry, it was no problem for Grundfos to construct the perfect solution.

But to replace a water treatment plant producing treated water for turbine operation is not something that you just do. Shutdown of boilers resulting in downtime is a serious operation that can take a very long time – operational disruptions that a CHP plant would very much like to avoid. Therefore, it was necessary to find a temporary solution to provide the right water quality during the replacement work.

Grundfos’ product range offers many construction options for rental units to solve specific problems. In this case, MEC's water requirements fitted well with a container solution combining reverse osmosis and an external mixed bed plant.

The cooperation with Grundfos

MEC invited offers from several suppliers, but the final choice fell on Grundfos. In particular, the thorough and accurate tender stood out among the rest. Everything was well thought out and the solution was ready to be carried out.

The support from Grundfos was impeccable – it has just been running along – a real textbook example. I will even say that this thoroughness I have not experienced before. It has given peace of mind in relation to further developments and operation.
Jørgen Pors-Nielsen

In informal settings, both parties discuss the next phase of the project: Membrane degassing of the district heating water instead of dosing to remove oxygen.

   

Facts

About the new water treatment plant

Nominal capacity: 

  • 12.5 m³/h

Units: 

  • DPRO C3-12/9 double-pass reverse osmosis system

  • EDI 3-5000e electronic deionization system

  • Lye dosing to remove CO2

About MEC

The plant currently supplies 28 MW of electricity corresponding to the consumption in approximately 40,000 households, and 84-110 MW of district heating corresponding to the heat consumption in 16-22,000 detached houses.

BioHeat & Power is a combined heat and power plant that supplies district heating and electricity to households in two Danish municipalities. BioGas is one of the world's largest industrial biogas plants and was commissioned in 2012. Together they form the Maabjerg Energy Center (MEC).

Over time, the ambition is to have a comprehensive sustainable energy solution based on local and CO2-neutral raw materials using the latest technologies.

Other related cases

Read related stories from customers who have also benefited from a Grundfos solution.