News
13-07-2022
Grundfos Ghana Water Initiative to roll out 12 new digital water sites
Following a successful pilot in Abomosu, the solar-powered, digitised water systems will provide access to clean water to over 100,000 people in underserved rural Ghana.
Following the success of its innovative smart tech clean water pilot in Abomosu, Grundfos Ghana Water Initiative (GWI) announced that it is developing 12 additional sites in collaboration with the Community Water and Sanitation Agency (CWSA) to give over 100,000 people across rural Ghana access to clean water by the end of 2023.
GWI, a project by Grundfos SafeWater, aims to reach one million people in underserved communities in Ghana with clean water by 2026, providing drinking water that is both safe and easily accessible, from a reliable source that is sustainable and efficiently run.
In 2019, GWI installed seven centrally located, solar-powered, digital AQTaps (water ATMs) to serve the first pilot community in Abomosu village, located in Atiwa West District, Eastern region of Ghana. The pilot was set upin partnership with the CWSA and the Atiwa West District Assembly.The innovative, ‘smart water’ ATMs allow the user to manage their usage, and access treated, potable water using a pre-paid card, topped up via mobile money, from a source that is reliable and accessible 24/7, all year round.
Today, safe running water is available throughout the community, pumped from a 90m borehole 1.5 km from the village to a 120m³ water tank. Over 8,000 local residents now have reliable access to clean water for the first time, including 262 smart household water connections going directly into residents’ homes.
Anise Sacranie, SafeWater’s Senior Partnership Development Manager commented: “We have demonstrated that this model is successful, so working closely with the CWSA, the next step is to take the model to scale, encouraging private sector engagement and entrepreneurship to establish financially sustainable, high-quality water services to underserved communities across Ghana.
We are about to finalise our next project (in Otoase) which is a completely new build and are on track to have a total of 13 projects running by the end of next year, including Abomosu, giving over 100,000 people access to clean drinking water within the next 18 months.”
Xorlali Yao-Kuma Kpodo, Grundfos Ghana Water Initiative’s Engagement Manager said, “Over 8 million people in Ghana still do not have access to safe, drinkable water because the current water supply in many areas is inefficient and untreated and therefore unsafe to drink when it flows. Since the start of the Abomosu pilot initiative 2 years ago, the feedback from local residents has been overwhelmingly positive so we are excited to be moving to the next phase, providing clean water to more underserved rural areas.”
The Ghana Water Initiative’s approach to improve water access is to either refurbish existing systems provided by the Community Water and Sanitation Agency or establish new infrastructures. The Abomosu project involved upgrading an existing system that had fallen into disrepair, requiring two new boreholes, piping, and treatment system, as well as the Grundfos AQ Taps.
About SafeWater:
SafeWater is a strategic business unit in Grundfos working with humanitarian partners around the world. The aim is to transform underserved communities through commercially viable and sustainable smart water solutions and to reach 10 million people annually with safely managed drinking water by 2025.
About Grundfos Ghana Water Initiative (GWI)
GWI began in March 2019 as a local initiative to test commercially viable business models for delivering clean water access to underserved communities in Ghana, and to establish the framework to take the final model to scale. GWI is being managed by a local project team working out of the Grundfos Ghana office in Accra. GWI aims to provide sustainable clean water that is accessible, reliable and efficient to one million Ghanaians by 2026 by rolling out successfully tested business models across Ghana.