- Grundfos
- Solutions
- Learn
- Ecademy
- All courses
- 13 - The Basic Hydraulics a...
- Test your knowledge
Question 1 of 8
Basic
Identify the reasons for reduction in pump performance from the given options:
Question 2 of 8
Basic
Which of the following items are built-in in some motors and can stop the motor if it exceeds a preset temperature:
Question 3 of 8
Basic
Identify the false statement.
Question 4 of 8
Basic
Identify the correct formula for calculating pump efficiency.
Question 5 of 8
Basic
Which of the following parameters is not used for calculating pump efficiency?
Question 6 of 8
Basic
What are the effects of cavitation on pumps?
Question 7 of 8
Basic
What causes cavitation?
Question 8 of 8
Basic
Friction loss is dependent on the [xxxxxxxx] of the fluid.
Question 8 of 8
Basic
Happy with your answers?
Submit your current answers and get the final test result.
Test results
Congratulations. You have passed the test and completed the 13 - The Basic Hydraulics and Pump Performance Course
Sorry. You did not pass the 13 - The Basic Hydraulics and Pump Performance Course test this time
Achieved badges:
How would you rate this course?
1: Identify the reasons for reduction in pump performance from the given options:
Bad power supply
1: Identify the reasons for reduction in pump performance from the given options:
Reduction in size of irrigation zone
You can find the answer here >
1: Identify the reasons for reduction in pump performance from the given options:
Changes in energy requirements
You can find the answer here >
2: Which of the following items are built-in in some motors and can stop the motor if it exceeds a preset temperature:
Temperature sensors
2: Which of the following items are built-in in some motors and can stop the motor if it exceeds a preset temperature:
Signal wire
You can find the answer here >
2: Which of the following items are built-in in some motors and can stop the motor if it exceeds a preset temperature:
Insulation system
You can find the answer here >
3: Identify the false statement.
Cavitation can occur when water is flowing in a pipe and a valve is closed too quickly.
3: Identify the false statement.
The MP204 device can protect the pump motor against all possible disturbances that may occur.
You can find the answer here >
3: Identify the false statement.
The only way to avoid sand from entering a pump is through effective filtering before the pump inlet.
You can find the answer here >
4: Identify the correct formula for calculating pump efficiency.
(P1 × Q)/(c × H)
You can find the answer here >
4: Identify the correct formula for calculating pump efficiency.
(p x H × Q)/(c × P1)
4: Identify the correct formula for calculating pump efficiency.
(H × P1)/(c × Q)
You can find the answer here >
5: Which of the following parameters is not used for calculating pump efficiency?
5: Which of the following parameters is not used for calculating pump efficiency?
Time
5: Which of the following parameters is not used for calculating pump efficiency?
Pressure
You can find the answer here >
5: Which of the following parameters is not used for calculating pump efficiency?
Power Consumption
You can find the answer here >
6: What are the effects of cavitation on pumps?
Breakage of rotor
You can find the answer here >
6: What are the effects of cavitation on pumps?
Pitting of suction pipe
You can find the answer here >
6: What are the effects of cavitation on pumps?
Pitting of impeller and pump housing
7: What causes cavitation?
Cavitation occurs when water changes its state from vapour to water at low pressure.
7: What causes cavitation?
Cavitation occurs when water boils at 100°C and changes its state from water to vapour at normal atmospheric pressure.
You can find the answer here >
7: What causes cavitation?
Cavitation occurs when water flows through a pipe and a valve is closed quickly at a low atmospheric pressure
You can find the answer here >
8: Friction loss is dependent on the [xxxxxxxx] of the fluid.
Viscosity
You can find the answer here >
8: Friction loss is dependent on the [xxxxxxxx] of the fluid.
Velocity
8: Friction loss is dependent on the [xxxxxxxx] of the fluid.