Make-up water for cooling tower
The water treatment solution provides 19 m³/h of make-up water for a cooling tower system at the company Messer Industriegase in the city of Speyer, Germany. Messer Industriegase is the largest privately held industrial gas business in the world.
Maintaining good water quality is essential to prevent scaling, corrosion, and biological fouling within the cooling tower. Utilizing demineralised water for cooling also reduce the frequency of blowdown significantly which lower the consumption of both water and energy. In this case, the required water quality is achieved by blending two water streams: partly filtered water and partly demineralised water.
The Messer Industriegase facility has its own private water supply from groundwater. First treatment step is iron removal in a Grundfos pressure filter. In case of insufficient supply from own source, the facility gets pretreated drinking water quality from the local waterworks.
The drinking water is stored in a 14 m³ clean water tank. Hereafter the water is demineralised in a Grundfos reverse osmosis unit with a capacity of 15 m³/h.