Research And Insight

Tandem seal

A tandem seal is the Grundfos name for a shaft seal system where an additional sealing chamber has been mounted on the existing shaft seal. The purpose of the sealing chamber in a tandem seal pump is to guarantee that liquid does not leak from the pump housing. By flushing the sealing chamber with a neutral fluid, excess fluid in the centrifugal pump is absorbed/removed.

Additional advantages

A Grundfos centrifugal pump with a tandem seal offers several advantages. The flushing fluid between the two seals is pressure-less and gives several advantages to the product-side shaft seal such as:

  • No evaporation in the sealing gap. This prevents the formation of deposits as well as crystallisation on the flushed fluid side
  • For liquid temperature between 120 °C and 150 °C a tandem seal can be used using cold liquid as flushing

Related products

Find products from Grundfos related to this subject.

Related applications

Find applications from Grundfos related to this subject.