FAQ

Question: Can I install a recirculation system in existing plumbing?

Answer:

In many cases, a household with a recirculation system can be retrofitted. However, the feasibility and ease of installation will depend on the layout of the plumbing system. It’s recommended to consult with a plumber or HVAC designer to assess the options.

Additional information: