FAQ
Question: Can SCALA pumps be used outdoors?
Answer:
Both SCALA pumps are IPX4D rated, meaning that the products can be installed outside. The pumps can be installed both indoors or outdoors, but it must not be exposed to frost. We recommend that you install the pump near a drain or in a drip tray connected to a drain to lead away possible condensation from cold surfaces. The product must be installed in a well-ventilated room to ensure cooling of its components. The installation location must be protected from rain, humidity, condensation, direct sunlight, and dust.