FAQ

Question: Can the SCALA pumps operate with hot water?

Answer:

The Grundfos SCALA1 and SCALA2 booster pumps can handle water temperatures ranging from 2°C to 45°C. This means they can be used for boosting cold water supplies in a domestic and residential setting.

This range covers typical temperatures for household water systems, but if your system involves extreme temperatures or has unique requirements, it's always recommended to consult with the manufacturer or a professional installer.

Always keep in mind that using these pumps outside of their designed operating conditions could lead to decreased performance and potential damage the pumps, voiding any warranties.

Additional information:

Get to know more about the product range or see more on SCALA1 or SCALA2