FAQ

Question: Do SCALA pumps create a lot of noise?

Answer:

The noise level of the Grundfos SCALA pumps is typically low and within acceptable limits for residential applications. SCALA2 is designed with a focus on reducing noise through features such as advanced motor technology and sound-dampening materials. It is engineered to operate quietly and provide a comfortable user experience.

Additional information:

Get to know more about the product range or see more on SCALA1 or SCALA2