FAQ
Question: How energy efficient are the SCALA pumps?
Answer:
SCALA pumps are designed to be energy efficient. The Grundfos SCALA2 is designed with energy efficiency as a key feature. It includes an Energy Efficiency Index (EEI) of ≤0.23, making it one of the most energy-efficient domestic booster pumps on the market.
Key features contributing to the SCALA2's energy efficiency include Intelligent Pump Control,, which adjusts the pump's operation according to water demand, Permanent Magnet Motor, which is more efficient than an induction motor, and Variable Speed Drive, which allows the pump to vary its speed in response to changing demand.
Please note that the actual energy consumption of the pump will depend on your specific usage patterns and the overall water demand in your home. Regular maintenance and correct installation also play crucial roles in ensuring the pump operates at its highest efficiency.