FAQ

Question: How much water can a recirculation system save?

Answer:

The amount of water and energy saved with a recirculation system depends on factors such as the size of the home, usage patterns, and the system’s efficiency. However, studies have shown that recirculation systems can save significant amounts of water and energy, often up to 10,000 gal. / 38,000 liters per year in a household.

Additional information: