FAQ
Question: How should I clean the integrated non-return valve?
Answer:
- Turn off the power supply and disconnect the power plug.
- Shut off the water source.
- Open the tap to release the pressure in the pipe system.
- Close the isolating valves and/or drain the pipes.
- Gradually open and remove the priming plug. The plug and non-return valve are one unit.
- Clean the integrated non-return valve with warm water and a soft brush.
- Assemble the components in reverse order.
Additional information:
Get to know more about the product range or see more on SCALA1 or SCALA2.