FAQ
Question: What applications is the UNILIFT APG suitable for?
Answer:
UNILIFT APG can be used in:
- Lifting stations inside buildings (typically basements below sewer level)
- Outdoor pumping stations connected to public sewer or pressure sewer systems
- Standalone pits in single houses
- One-family houses (single pump) or multi-family/low-rise buildings (dual-pump systems)
Additional information:
Download the UNILIFT Range Selection Guide or find more information about the range here.