FAQ

Question: When should I choose a grinder pump like APG instead of a standard drainage effluent pump?

Answer:

Choose APG when the installation includes:

  • Blackwater (toilet discharge)
  • Need to pump through small pipes (DN32/DN40)
  • Long horizontal/vertical distances
  • No gravity sewer available (basements, rural houses)

Additional information:

Download the UNILIFT Range Selection Guide or find more information about the range here.