FAQ
Question: Which pump should I use for emptying a tank, pool or pond?
Answer:
Use a portable submersible pump:
- UNILIFT CC
- UNILIFT KP
- UNILIFT AP
The UNILIFT CC can drain water down to 3 mm when the strainer is removed.
Additional information:
Download the UNILIFT Range Selection Guide or find more information about the range here.