FAQ
Question: Why does the UNILIFT pump stop shortly after starting?
Answer:
Common causes:
- Thermal relay in starter is set too low → Adjust according to pump nameplate.
- Low voltage / excessive voltage drop → Measure phase voltage and ensure deviation is within ±10%.
- Blocked impeller causing overload → Clean the impeller.
Additional information:
Need more support? Check out the UNILIFT range course at Ecademy; our free online training tool.
Or find more product information here.