Search for quick guides, manuals and more

Reset search
Showing 111 to 120 of 149 results
Search for quick guides, manuals and more
Back-to-back seal
A back-to-back seal describes two shaft seals mounted back-to-back to provide a higher level of safety and reliability.
Baffle
The term baffle covers a flat board or plate, deflector vanes, guides, grids, gratings or similar devices constructed or placed in flowing water, wastewater or slurry systems.
Balance point
In any thermal heat exchange process, a mixture of two energy flows will result in a new stage or phase called the balance point. Here, a common temperature, humidity or enthalpy is reached.
Balancing valve
During commissioning of heating and cooling systems, hydraulic balance is often achieved using balancing valves; static or dynamic
Balancing
Balancing of heating and cooling systems is performed to ensure that the correct amount of water is present at all consumption points. Balancing is carried out by building balancing valves into the system, thereby adding adjustable resistance.
Biocide
Biocide is a chemical added to the make-up water for evaporative applications such as condensers and cooling towers.
Biofilm
Biofilm refers to a population of various micro-organisms trapped in a layer of slime and organic matter that attaches itself to the surfaces of pumps, pipes, walls etc.
BOD (Biochemical Oxygen Demand)
The quantity of oxygen consumed by aerobic microorganisms during the decomposition of organic matter in a water sample is defined as the Biochemical Oxygen Demand (BOD).
Boiler shunt
The primary task of the boiler shunt is to ensure that the difference in temperature between the top and the bottom of the boiler is not too high. A high temperature difference can cause tensions in the material and thus reduce the life of the boiler.
BMS (Building Management System)
A BMS is an integrated data network and control system for automation, monitoring and control of HVAC, lighting and other functions in a building.